EEO#.PIN
Description
EEO#.PIN is used in conjunction with EEO#.POUT to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-07-00-000 |
General Information
Type | Read/Write |
Description | Sets the gear IN of the EEO position |
Units | N/A |
Range | 1 to 4,294,967,295 |
Default Value | 1 |
Data Type | Integer |
See Also | EEO#.POUT |
Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
EEO1.PIN |
4600h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
EEO2.PIN |
4601h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
EEO3.PIN |
4603h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
EEO4.PIN |
4606h |
08h |
Unsigned32 |
- |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
32045 |
1 |
32045 (0x7d2d) |
EEO1.PIN |
Unsigned32 |
Read/Write |
Yes |
32046 |
1 |
32046 (0x7d2e) |
EEO2.PIN |
Unsigned32 |
Read/Write |
Yes |
32047 |
1 |
32047 (0x7d2f) |
EEO3.PIN |
Unsigned32 |
Read/Write |
Yes |
32048 |
1 |
32048 (0x7d30) |
EEO4.PIN |
Unsigned32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
EEO1.PIN |
32045 |
Unsigned32 |
Read/Write |
- |
EEO2.PIN |
32046 |
Unsigned32 |
Read/Write |
- |
EEO3.PIN |
32047 |
Unsigned32 |
Read/Write |
- |
EEO4.PIN |
32048 |
Unsigned32 |
Read/Write |
- |